IrayPlusMaterialAttributeEnum Class¶
-
class
NXOpen.Display.
IrayPlusMaterialAttributeEnum
¶ Bases:
NXOpen.Display.IrayPlusMaterialAttribute
Represents a IrayPlus Enum Attribute
This class is restricted to being called from a program running during an Interactive NX session. If run from a non-interactive session it will return None.
IrayPlusMaterialAttributeEnum is not supported in KF.
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
EnumValue | Returns or sets the enum value |
ParameterName | Returns or sets the parameter name of specific material object. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetValueAsString | Gets an attribute’s value as string for specific attribute object The attribute object can be queried from function: NXOpen.Display.IrayPlusMaterialEditorBuilder.GetComponentParameter() . |
SetValueFromString | Sets attribute’s value for specific attribute object. |
Property Detail¶
EnumValue¶
-
IrayPlusMaterialAttributeEnum.
EnumValue
¶ Returns or sets the enum value
-------------------------------------
Getter Method
Signature
EnumValue
Returns: Return type: int New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumValue
Parameters: enumValue (int) – New in version NX12.0.0.
License requirements: None.