ImageDataCollection Class¶
-
class
NXOpen.Display.
ImageDataCollection
¶ Bases:
object
Represents a collection of
NXOpen.Display.ImageData
objects.The
NXOpen.Display.ImageDataCollection
also provides an iterator that iterates through all theNXOpen.Display.ImageData
objects in the part.To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.Display.ImageData with the given identifier as recorded in a journal. |
Method Detail¶
FindObject¶
-
ImageDataCollection.
FindObject
¶ Finds the
NXOpen.Display.ImageData
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general,this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: Image data found Return type: NXOpen.Display.ImageData
New in version NX9.0.0.
License requirements: None.