ImageBasedLightingImagesType Enumeration¶
NXOpen.Display.ImageBasedLighting.ImagesType is an alias for NXOpen.Display.ImageBasedLightingImagesType
-
class
NXOpen.Display.
ImageBasedLightingImagesType
¶ Bases:
object
images type - environment used for generating image-based lighting
Enum Members
Enum Member Enum Member Description Background Use the background image. Stage Use the stage. UserDefined Use the image file specified. LightingOnly only used for IBL -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-