IRayPlusStudioEditorBuilderIRayPlusStudioStaticImageSizeType Enumeration¶
NXOpen.Display.IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageSizeType is an alias for NXOpen.Display.IRayPlusStudioEditorBuilderIRayPlusStudioStaticImageSizeType
-
class
NXOpen.Display.
IRayPlusStudioEditorBuilderIRayPlusStudioStaticImageSizeType
¶ Bases:
object
To specify the Ray Traced Studio static image size
Enum Members
Enum Member Enum Member Description RenderWindow Ray Traced Studio window size used for static image output UserDefined user specified size for static image output -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-