IRayPlusStudioEditorBuilderIRayPlusStudioStaticImageOrientationType Enumeration¶
NXOpen.Display.IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageOrientationType is an alias for NXOpen.Display.IRayPlusStudioEditorBuilderIRayPlusStudioStaticImageOrientationType
-
class
NXOpen.Display.
IRayPlusStudioEditorBuilderIRayPlusStudioStaticImageOrientationType
¶ Bases:
object
To specify the Ray Traced Studio static image orientation
Enum Members
Enum Member Enum Member Description Landscape static image orientation where width is greater than height Portrait static image orientation where height is greater than width -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-