IRayPlusStudioEditorBuilderIRayPlusStudioRemoteRenderVideoType Enumeration¶
NXOpen.Display.IRayPlusStudioEditorBuilder.IRayPlusStudioRemoteRenderVideoType is an alias for NXOpen.Display.IRayPlusStudioEditorBuilderIRayPlusStudioRemoteRenderVideoType
-
class
NXOpen.Display.
IRayPlusStudioEditorBuilderIRayPlusStudioRemoteRenderVideoType
¶ Bases:
object
To specify the Ray Traced Studio remote rendering video mode
Deprecated since version NX12.0.0: This is removed. The video mode is determined by the Ray Traced Studio render mode.
Enum Members
Enum Member Enum Member Description Streaming Synchronous -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-