IRayPlusStudioEditorBuilderDynamicIRayPlusStudioRenderModeType Enumeration¶
NXOpen.Display.IRayPlusStudioEditorBuilder.DynamicIRayPlusStudioRenderModeType is an alias for NXOpen.Display.IRayPlusStudioEditorBuilderDynamicIRayPlusStudioRenderModeType
-
class
NXOpen.Display.
IRayPlusStudioEditorBuilderDynamicIRayPlusStudioRenderModeType
¶ Bases:
object
To specify the quality and performance of the Ray Traced Studio display when dynamic interaction stops
Enum Members
Enum Member Enum Member Description Photoreal Very good ray traced display quality when dynamic interaction stops QualityInteractive Good ray traced display quality with good performance when dynamic interaction stops FastInteractive The fastest ray traced display performance with preview quality when dynamic interaction stops -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-