FacetSettingsBuilderShadedToleranceSetting Enumeration¶
NXOpen.Display.FacetSettingsBuilder.ShadedToleranceSetting is an alias for NXOpen.Display.FacetSettingsBuilderShadedToleranceSetting
-
class
NXOpen.Display.
FacetSettingsBuilderShadedToleranceSetting
¶ Bases:
object
Specifies which set of tolerances are to be used for rendering facets for display for Shaded views.
Enum Members
Enum Member Enum Member Description Coarse Standard Fine ExtraFine UltraFine UserDefined -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-