FacetSettingsBuilderFacetToViewRatio Enumeration¶
NXOpen.Display.FacetSettingsBuilder.FacetToViewRatio is an alias for NXOpen.Display.FacetSettingsBuilderFacetToViewRatio
-
class
NXOpen.Display.
FacetSettingsBuilderFacetToViewRatio
¶ Bases:
object
Specifies whether the ratio of the view scale to the scale used to generate facets is determined automatically by the system (as was always done before NX 8) or whether a ratio defined by the user (by one of the set_*FacetRatio methods) is to be used as the ratio.
Deprecated since version NX9.0.0: Refer to
NXOpen.Display.FacetSettingsBuilderFacetScale
insteadEnum Members
Enum Member Enum Member Description Automatic UserDefined -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-