DynamicSectionTypesCurveColorOption Enumeration¶
NXOpen.Display.DynamicSectionTypes.CurveColorOption is an alias for NXOpen.Display.DynamicSectionTypesCurveColorOption
-
class
NXOpen.Display.
DynamicSectionTypesCurveColorOption
¶ Bases:
object
Specifies the color of the curves created by the section plane. When color is set to body color, user specified color will be ignored.
Enum Members
Enum Member Enum Member Description Body Use body color Any Use specified color -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-