DynamicSectionTypesCoordinateSystem Enumeration¶
NXOpen.Display.DynamicSectionTypes.CoordinateSystem is an alias for NXOpen.Display.DynamicSectionTypesCoordinateSystem
-
class
NXOpen.Display.
DynamicSectionTypesCoordinateSystem
¶ Bases:
object
Specifies the coordinate system used for creating principal planes i.e. X, Y, Z planes. Note that the coordinate system is only used during plane creation to set initial reference. When using WCS, the X plane will be created such that its normal aligns with WCS X direction.
All APIs that accept/receive geometric works in absolute coordinates.
Enum Members
Enum Member Enum Member Description Absolute Absolute Wcs WCS -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-