DynamicSectionTypesCapColorOption Enumeration¶
NXOpen.Display.DynamicSectionTypes.CapColorOption is an alias for NXOpen.Display.DynamicSectionTypesCapColorOption
-
class
NXOpen.Display.
DynamicSectionTypesCapColorOption
¶ Bases:
object
Specifies cap color type to be used for the cap. When cap color type is body, then user-specified color is ignored.
Enum Members
Enum Member Enum Member Description Body Use body color Any User-specified color is used -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-