DecalBuilderScaling Enumeration¶
NXOpen.Display.DecalBuilder.Scaling is an alias for NXOpen.Display.DecalBuilderScaling
-
class
NXOpen.Display.
DecalBuilderScaling
¶ Bases:
object
decal scaling type
Enum Members
Enum Member Enum Member Description ToFace scale the decal based on face size ToImageSize scale the decal based on true decal image size ToUniformScale scale the decal based on uniform scale ToNonUniformScale scale the decal based on both width and height scale -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-