DecalBuilderImageSize Enumeration¶
NXOpen.Display.DecalBuilder.ImageSize is an alias for NXOpen.Display.DecalBuilderImageSize
-
class
NXOpen.Display.
DecalBuilderImageSize
¶ Bases:
object
image size type
Enum Members
Enum Member Enum Member Description TrueSize use true image size OneTwentyEight resize image to 128 x 128 TwoFiftySix resize iamge to 256 x 256 FiveTwelve resize image to 512 x 512 OneOTwoFour resize image to 1024 x1024 TwoOFourEight resize image to 2048x2048 FourONineSix resize image to 4096x 4096 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-