DecalBuilderAnchor Enumeration¶
NXOpen.Display.DecalBuilder.Anchor is an alias for NXOpen.Display.DecalBuilderAnchor
-
class
NXOpen.Display.
DecalBuilderAnchor
¶ Bases:
object
image anchor
Enum Members
Enum Member Enum Member Description TopLeft anchor at top left corner of decal image Center anchor in the middle of decal image BottomLeft anchor at the bottom left corner of decal image TopMiddle anchor at top middle corner of decal image TopRight anchor at top right corner of decal image LeftMiddle anchor at left middle corner of decal image RightMiddle anchor at right middle corner of decal image BottomMiddle anchor at bottom middle corner of decal image BottomRight anchor at bottom right corner of decal image -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-