CanonMRTestBuilderImageUsageType Enumeration¶
NXOpen.Display.CanonMRTestBuilder.ImageUsageType is an alias for NXOpen.Display.CanonMRTestBuilderImageUsageType
-
class
NXOpen.Display.
CanonMRTestBuilderImageUsageType
¶ Bases:
object
Indicates how the image identified by ImageFile is specified to CGP.
Enum Members
Enum Member Enum Member Description NotSet The image is ignored, so neither background nor foreground is displayed. Dual The image is specified as a dual image that is displayed as both the background and foreground. Background3Only The image is specified as a BGR or RGB background image only, so no foreground is displayed. Background4Only The image is specified as a BGRA or RGBA background image only, so no foreground is displayed. Background3AndForeground The image is specified separately as a BGR or RGB background image and a foreground image. Background4AndForeground The image is specified separately as a BGRA or RGBA background image and a foreground image. ForegroundOnly The image is specified as a foreground image only, so no background is displayed. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-