CameraBuilderLensFlare Enumeration¶
NXOpen.Display.CameraBuilder.LensFlare is an alias for NXOpen.Display.CameraBuilderLensFlare
-
class
NXOpen.Display.
CameraBuilderLensFlare
¶ Bases:
object
Predefined lens flare types: Standard, 35mm, 50mm, 105mm, polygonal, 35mm poly, 50mm poly, 105mm poly, spark, star
Enum Members
Enum Member Enum Member Description Standard Standard lens S35 35mm S50 50mm S105 105mm Polygonal polygonal P35 35mm poly P50 50mm poly P105 105mm poly Spark spark lens Star star lens -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-