BoundedGridBuilderLabelReferenceType Enumeration¶
NXOpen.Display.BoundedGridBuilder.LabelReferenceType is an alias for NXOpen.Display.BoundedGridBuilderLabelReferenceType
-
class
NXOpen.Display.
BoundedGridBuilderLabelReferenceType
¶ Bases:
object
Specifies label reference.
Enum Members
Enum Member Enum Member Description Local Use local grid origin to determine grid line offset labels Wcs Use projection of WCS origin on the grid plane to determine grid line offset labels Absolute Use projection of absolute origin on the grid plane to determine grid line offset labels -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-