DirectionOnFaceOption Enumeration¶
NXOpen.Direction.OnFaceOption is an alias for NXOpen.DirectionOnFaceOption
-
class
NXOpen.
DirectionOnFaceOption
¶ Bases:
object
Specifies the direction in relation to a face.
Enum Members
Enum Member Enum Member Description IsoU Creates direction in U parameter direction on face. IsoV Creates direction in V parameter direction on face. Normal Creates direction normal to face. Section Creates direction in a sectional direction to face. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-