AddSurfBuilderMethods Enumeration |
Settings for the type of addendum surface being created. |
AddendumSectionBuilderSectionLocationType Enumeration |
The settings indicating the location of the section being created. |
AddendumSectionBuilderSectionOrientationType Enumeration |
The settings to indicate the section orientation. |
AddendumSectionBuilderSectionShapeType Enumeration |
The settings to indicate the section shape. |
AddendumSectionBuilderSegmentParameterType Enumeration |
The settings to indicate which parameter of the segment to lock. |
AddendumSectionBuilderSegmentType Enumeration |
The settings to indicate the segment type to update. |
AddendumSectionBuilderSurfaceBuildType Enumeration |
The settings to indicate the surface type. |
ClampingSlotBuilderTypes Enumeration |
Clamping slot types |
ClearanceBuilderClearanceGeometryTypes Enumeration |
Identifies which type of input defines the clearance. |
ClearanceBuilderTypes Enumeration |
Identifies which clearance type is being created in the casting. |
CompensateRoughDataBuilderApproximationType Enumeration |
Settings for the amount of approximation to perform. |
CompensateRoughDataBuilderTypes Enumeration |
Settings for the type of data being compensated. |
DieAssistantFlangeProfileType Enumeration |
Settings for the flange type. |
DieBooleanBuilderBooleanType Enumeration |
boolean type to apply to the selected solids |
DieBuildStatusOption Enumeration |
Settings for the build status of the die design sub features. |
DieDirectionBuilderDirectionType Enumeration |
the options available for defining the direction |
DieLocationBuilderLocationType Enumeration |
the options available for defining the location |
DiePlaneBuilderPlaneType Enumeration |
the options available for defining the plane |
DirectionOption Enumeration |
Settings for the profile direction. |
DrawBeadBuilderFemaleDepthTypes Enumeration |
Specifies how the female depth is calculated or defined. |
DrawBeadBuilderFemaleWidthTypes Enumeration |
Specifies how the feamle width is calcualted or defined. |
DrawBeadBuilderMaleBeadPositionTypes Enumeration |
Identifes which casting the male bead is created in. |
DrawBeadBuilderOrientSectionToDrawTypes Enumeration |
Specifies if the segment height section parameter should be oriented to the draw direction or the sheet metal normal at the section location. |
DrawBeadBuilderOrientationTypes Enumeration |
Identifies the orientation of the base parameters to the sheet metal. |
DrawBeadBuilderOutputTypes Enumeration |
Specifies what type of output is desired for the feature creation. |
DrawBeadBuilderProjectionDirectionTypes Enumeration |
Identifes how the centerline should be projected to the placement face during processing. |
DrawBeadBuilderTransitionDefinitionTypes Enumeration |
Specifies how the transition area should be determined from segment to segment within a single bead. |
DrawBeadSegmentBuilderMaleBeadWidthTypes Enumeration |
value for how the male width is specified. |
DrawBeadTaperBuilderTaperTypes Enumeration |
Taper types to define how the slope is created for the bead end. |
FillAreaBuilderTypes Enumeration |
Identifies the area of the casting the fill is targeted for. |
FillAreaBuilderUpperLimitTypes Enumeration |
Specifies how the upper limit of the fill area is defined. |
FingerClearanceNotchBuilderTypes Enumeration |
Specifies what type of base geometry to build the finger clearance notch from. |
FlangeTaskBuilderCamTypes Enumeration |
Settings for the cam type of the flange task. |
FlangeTaskBuilderPierceTypes Enumeration |
Settings for the pierce type of the flange task. |
FlangeTaskBuilderSpringbackTypes Enumeration |
Settings for the springback type of the flange task. |
HandlingCoreBuilderTypes Enumeration |
Identifies how the handling Core is located in space. |
HeelpostBuilderTypes Enumeration |
Heelpost types |
KeywayBuilderLocationType Enumeration |
Keyway location direction relative to the die centerline coordinate system |
KeywayBuilderTypes Enumeration |
Keyway runoff types |
KeywayChildBuilderLocationOption Enumeration |
Settings for the location of the keyway. |
KeywayChildBuilderRunoffTypeOption Enumeration |
Settings for the runoff type of the keyway. |
KeywayParentBuilderRunoffTypeOption Enumeration |
Settings for the runoff type of the keyway. |
MachineReliefBuilderMainProfileTypes Enumeration |
Specifies that the profile is for an exterior or interior profile. |
MachineReliefBuilderTrimSheetTypes Enumeration |
Specifies what the trimming surface is defined by. |
MachineReliefBuilderTypes Enumeration |
Identifies the type of structure to be added, or subtracted, to the casting. |
OutputCurvesBuilderSmoothTypes Enumeration |
Settings for the curve smoothing type. |
OutputCurvesBuilderTrimCurveCreateTypes Enumeration |
Settings for the trim curve creation type. |
OutputCurvesBuilderTrimCurveTypes Enumeration |
Settings for the trim curve type. |
OutputCurvesBuilderTrimOutputCurveTypes Enumeration |
Settings for the trim curve output type. |
PadChildBuilderShapeTypeOption Enumeration |
Settings for the shape type of the die pad. |
PadParentBuilderShapeTypeOption Enumeration |
Settings for the shape type of the die pads. |
PierceHoleChildBuilderShapeTypeOption Enumeration |
Settings for the shape type of the pierce hole. |
PierceItemBuilderHoleShapeType Enumeration |
Settings for the hole shape of individual pierces. |
PierceItemBuilderSizingMethodOption Enumeration |
Settings for the sizing method of individual pierces. |
PierceTaskBuilderCamTypes Enumeration |
Settings for the cam type of the pierce task. |
PierceTaskBuilderCenterPointOptionTypes Enumeration |
Settings for the center point output options of the pierce task. |
PierceTaskBuilderPrecisionTypes Enumeration |
Settings for the precistion type of the pierce task. |
QuickBinderBuilderEditTypes Enumeration |
The type of edit to be performed on the face. |
QuickBinderBuilderTypes Enumeration |
The method used to approximate the product faces. |
QuickBinderWrapBuilderEditSizeType Enumeration |
Settings for the edit size type. |
QuickBinderWrapBuilderTypes Enumeration |
Settings for the binder wrap sheet body type. |
SpringbackCompensationBuilderDefinedByType Enumeration |
The type of input data that defines the compensation. |
SpringbackCompensationBuilderDegreeType Enumeration |
The polynomial degree type. |
SpringbackCompensationBuilderResultSheetType Enumeration |
The type of sheet body you would like created as output. |
SteelInsertBuilderInsertTypeOption Enumeration |
Settings for the insert type. |
SteelInsertSectionBuilderExtensionTypeOption Enumeration |
Settings for the extension type. |
SteelInsertSegmentChildBuilderExtensionTypeOption Enumeration |
Settings for the extension type. |
SteelInsertSegmentChildBuilderInsertTypeOption Enumeration |
Settings for the insert type. |
SteelInsertSegmentParentBuilderExtensionTypeOption Enumeration |
Settings for the extension type. |
SteelInsertSegmentParentBuilderInsertTypeOption Enumeration |
Settings for the insert type. |
ThroatChildBuilderTypeOption Enumeration |
Settings for the type of the throat section. |
ThroatParentBuilderTypeOption Enumeration |
Settings for the type of the throat section. |
TrimLineDevelopmentBuilderConvergency Enumeration |
The solver convergency level of onestep unform. |
TrimLineDevelopmentBuilderMaterialTypeName Enumeration |
Indicates type of material |
TrimLineDevelopmentBuilderMeshElement Enumeration |
The 2-D mesh element type of onestep unform. |
TrimLineDevelopmentBuilderOutputMethodName Enumeration |
Indicates which trim curves to output |
TrimLineDevelopmentBuilderSmoothingName Enumeration |
Indicates type of curve smoothing |
TrimLineDevelopmentBuilderSurface Enumeration |
The surface types of onestep unform. |
TrimTaskBuilderCamTypes Enumeration |
Settings for the cam type of the trim task. |
TrimTaskBuilderMatchCutTypes Enumeration |
Settings for the match cut type of the trim task. |
UncutRegionsBuilderResultsType Enumeration |
Indicates which side of curve to check |
WearPlateLocChildBuilderPositionType Enumeration |
Settings for the positioning of the locator relative to the wear plate. |
WearPlateLocParentBuilderPositionType Enumeration |
Settings for the positioning of the locator relative to the wear plate. |