WearPlateLocChildBuilderPositionType Enumeration¶
NXOpen.Die.WearPlateLocChildBuilder.PositionType is an alias for NXOpen.Die.WearPlateLocChildBuilderPositionType
-
class
NXOpen.Die.
WearPlateLocChildBuilderPositionType
¶ Bases:
object
Settings for the positioning of the locator relative to the wear plate.
Enum Members
Enum Member Enum Member Description Left Position locator to the left of the wear plate. Right Position locator to the right of the wear plate. Both Position locator on both sides of the wear plate. Neither No locators. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-