TrimLineDevelopmentBuilderOutputMethodName Enumeration¶
NXOpen.Die.TrimLineDevelopmentBuilder.OutputMethodName is an alias for NXOpen.Die.TrimLineDevelopmentBuilderOutputMethodName
-
class
NXOpen.Die.
TrimLineDevelopmentBuilderOutputMethodName
¶ Bases:
object
Indicates which trim curves to output
Enum Members
Enum Member Enum Member Description Geometric Geometric curve only Corrected Corrected curve only Both Both geometric and corrected curves -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-