TrimLineDevelopmentBuilderConvergency Enumeration

NXOpen.Die.TrimLineDevelopmentBuilder.Convergency is an alias for NXOpen.Die.TrimLineDevelopmentBuilderConvergency

class NXOpen.Die.TrimLineDevelopmentBuilderConvergency

Bases: object

The solver convergency level of onestep unform.

Enum Members

Enum Member Enum Member Description
Low Onestep solver convergency level is low
Medium Onestep solver convergency level is medium
High Onestep solver convergency level is high
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.