ThroatParentBuilderTypeOption Enumeration¶
NXOpen.Die.ThroatParentBuilder.TypeOption is an alias for NXOpen.Die.ThroatParentBuilderTypeOption
-
class
NXOpen.Die.
ThroatParentBuilderTypeOption
¶ Bases:
object
Settings for the type of the throat section.
Enum Members
Enum Member Enum Member Description Wipe Throat is built for a wipe operation. Restrike Throat is built for a restrike operation. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-