SpringbackCompensationBuilderDegreeType Enumeration¶
NXOpen.Die.SpringbackCompensationBuilder.DegreeType is an alias for NXOpen.Die.SpringbackCompensationBuilderDegreeType
-
class
NXOpen.Die.
SpringbackCompensationBuilderDegreeType
¶ Bases:
object
The polynomial degree type. Acceptable degrees are 2, 3, 5, and 7.
Enum Members
Enum Member Enum Member Description Two Degree is 2 Three Degree is 3 Five Degree is 5 Seven Degree is 7 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-