QuickBinderBuilderEditTypes Enumeration¶
NXOpen.Die.QuickBinderBuilder.EditTypes is an alias for NXOpen.Die.QuickBinderBuilderEditTypes
-
class
NXOpen.Die.
QuickBinderBuilderEditTypes
¶ Bases:
object
The type of edit to be performed on the face.
Enum Members
Enum Member Enum Member Description EdgeExtend Extend edge of a face. EdgeExtendStart Extend start edge of a planar face. EdgeExtendEnd Extend end edge of a planar face. EdgeAngleStart Change the angle of the start edge of a planar face. EdgeAngleEnd Change the angle of the end edge of a planar face. FaceRadius Change the face radius of a conical/cylindrical face. FaceCentralAngle Change the central angle of a conical/cylindrical face. FaceReverseConvexity Reverse the convexity of a conical/cylindrical face. Transform Transform body. ExtendUMinimum Extend the U Minimum edge of the anchor face. ExtendUMaximum Extend the U Maximum edge of the anchor face. ExtendVMinimum Extend the V Minimum edge of the anchor face. ExtendVMaximum Extend the V Maximum edge of the anchor face. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-