PressModelRoot Class

class NXOpen.Die.PressModelRoot

Bases: NXOpen.TaggedObject

Represents a Die Simulation - Press Model Root.

This class never built directly by the customer.

New in version NX6.0.0.

Properties

Property Description
Tag Returns the Tag for this object.

Methods

Method Description
IsActive Is the press model active

Method Detail

IsActive

PressModelRoot.IsActive

Is the press model active

Signature IsActive()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: ug_die_design (“Die Design”)