OutputCurvesBuilderTrimOutputCurveTypes Enumeration¶
NXOpen.Die.OutputCurvesBuilder.TrimOutputCurveTypes is an alias for NXOpen.Die.OutputCurvesBuilderTrimOutputCurveTypes
-
class
NXOpen.Die.
OutputCurvesBuilderTrimOutputCurveTypes
¶ Bases:
object
Settings for the trim curve output type.
New in version NX4.0.1.
Enum Members
Enum Member Enum Member Description Geometric Geometric. Corrected Corrected. Both Both geometric and corrected. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-