MachineReliefBuilderTypes Enumeration¶
NXOpen.Die.MachineReliefBuilder.Types is an alias for NXOpen.Die.MachineReliefBuilderTypes
-
class
NXOpen.Die.
MachineReliefBuilderTypes
¶ Bases:
object
Identifies the type of structure to be added, or subtracted, to the casting.
Enum Members
Enum Member Enum Member Description Cam Add casting material for the trim, or flange, steel mating surface. Relief Remove casting material to allow for clearance between two mating objects (such as the upper and lower castings). Thicken Add casting material to thicken an existing wall. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-