MachineReliefBuilderTrimSheetTypes Enumeration¶
NXOpen.Die.MachineReliefBuilder.TrimSheetTypes is an alias for NXOpen.Die.MachineReliefBuilderTrimSheetTypes
-
class
NXOpen.Die.
MachineReliefBuilderTrimSheetTypes
¶ Bases:
object
Specifies what the trimming surface is defined by.
Enum Members
Enum Member Enum Member Description Sheet Trimming surface is a sheet body. Face Trimming surface is a face, or faces to be sewed together. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-