KeywayChildBuilderLocationOption Enumeration¶
NXOpen.Die.KeywayChildBuilder.LocationOption is an alias for NXOpen.Die.KeywayChildBuilderLocationOption
-
class
NXOpen.Die.
KeywayChildBuilderLocationOption
¶ Bases:
object
Settings for the location of the keyway.
Enum Members
Enum Member Enum Member Description PositiveX Keyway built in positive x direction. NegativeX Keyway built in negative x direction. PositiveY Keyway built in positive y direction. NegativeY Keyway built in negative y direction. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-