KeywayBuilderLocationType Enumeration¶
NXOpen.Die.KeywayBuilder.LocationType is an alias for NXOpen.Die.KeywayBuilderLocationType
-
class
NXOpen.Die.
KeywayBuilderLocationType
¶ Bases:
object
Keyway location direction relative to the die centerline coordinate system
Enum Members
Enum Member Enum Member Description PositiveX +X relative to the center of the coordinate system NegativeX -X relative to the center of the coordinate system PositiveY +Y relative to the center of the coordinate system NegativeY -Y relative to the center of the coordinate system -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-