HeelpostBuilderTypes Enumeration¶
NXOpen.Die.HeelpostBuilder.Types is an alias for NXOpen.Die.HeelpostBuilderTypes
-
class
NXOpen.Die.
HeelpostBuilderTypes
¶ Bases:
object
Heelpost types
Enum Members
Enum Member Enum Member Description GuidepostWearplate allows a guide pin hole to be created StorageBlock no hole allowed SafetyBlock no hole allowed -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-