HandlingCoreBuilderTypes Enumeration¶
NXOpen.Die.HandlingCoreBuilder.Types is an alias for NXOpen.Die.HandlingCoreBuilderTypes
-
class
NXOpen.Die.
HandlingCoreBuilderTypes
¶ Bases:
object
Identifies how the handling Core is located in space.
Enum Members
Enum Member Enum Member Description AtLocation Location specified by the user. FromBase Location is an offset from the base. MapFromBase Locate by finding the minimum distance to the main profile of the target and then project and offset from the base. Used specifically for coring the main wall. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-