FlangeTaskBuilderPierceTypes Enumeration¶
NXOpen.Die.FlangeTaskBuilder.PierceTypes is an alias for NXOpen.Die.FlangeTaskBuilderPierceTypes
-
class
NXOpen.Die.
FlangeTaskBuilderPierceTypes
¶ Bases:
object
Settings for the pierce type of the flange task.
Enum Members
Enum Member Enum Member Description Gage Use Gage tolerance. Critical Use Critical tolerance. Standard Use Standard tolerance. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-