FlangeTaskBuilderCamTypes Enumeration¶
NXOpen.Die.FlangeTaskBuilder.CamTypes is an alias for NXOpen.Die.FlangeTaskBuilderCamTypes
-
class
NXOpen.Die.
FlangeTaskBuilderCamTypes
¶ Bases:
object
Settings for the cam type of the flange task.
Enum Members
Enum Member Enum Member Description Direct Direct AerialConventional Aerial Cam - Conventional Fill BaseConventional Base Mounted Cam - Conventional Fill AerialRotary Aerial Cam - Rotary Fill BellCrank Bell Crank -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-