FingerClearanceNotchBuilderTypes Enumeration¶
NXOpen.Die.FingerClearanceNotchBuilder.Types is an alias for NXOpen.Die.FingerClearanceNotchBuilderTypes
-
class
NXOpen.Die.
FingerClearanceNotchBuilderTypes
¶ Bases:
object
Specifies what type of base geometry to build the finger clearance notch from.
Enum Members
Enum Member Enum Member Description Section Build from an open section profile. Face Build from either a single face or a set of connected faces. SheetBody Build from either a sheet body or a solid body. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-