DrawBeadTaperBuilderTaperTypes Enumeration¶
NXOpen.Die.DrawBeadTaperBuilder.TaperTypes is an alias for NXOpen.Die.DrawBeadTaperBuilderTaperTypes
-
class
NXOpen.Die.
DrawBeadTaperBuilderTaperTypes
¶ Bases:
object
Taper types to define how the slope is created for the bead end.
Enum Members
Enum Member Enum Member Description Spherical Create a spherical end based on a radius. Washout Create a slope based on the height and length desired. Point Use the spherical method, but the radius is defined by a point location and distance to the end of the centerline. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-