DrawBeadSegmentBuilderMaleBeadWidthTypes Enumeration¶
NXOpen.Die.DrawBeadSegmentBuilder.MaleBeadWidthTypes is an alias for NXOpen.Die.DrawBeadSegmentBuilderMaleBeadWidthTypes
-
class
NXOpen.Die.
DrawBeadSegmentBuilderMaleBeadWidthTypes
¶ Bases:
object
value for how the male width is specified.
Enum Members
Enum Member Enum Member Description Constant The male bead width is specified by a constant value. Derived The male bead width is derived from the width specified for the female. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-