DiePlaneBuilderPlaneType Enumeration¶
NXOpen.Die.DiePlaneBuilder.PlaneType is an alias for NXOpen.Die.DiePlaneBuilderPlaneType
-
class
NXOpen.Die.
DiePlaneBuilderPlaneType
¶ Bases:
object
the options available for defining the plane
Enum Members
Enum Member Enum Member Description Selection Select the plane to be used. Plane Define the plane to be used. CoordinateSystem Define a coordinate system to specify the plane. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-