DieLocationBuilderLocationType Enumeration¶
NXOpen.Die.DieLocationBuilder.LocationType is an alias for NXOpen.Die.DieLocationBuilderLocationType
-
class
NXOpen.Die.
DieLocationBuilderLocationType
¶ Bases:
object
the options available for defining the location
Enum Members
Enum Member Enum Member Description SelectLocation Select the point to be used. NewPoint Define the point to be used. NewCoordinateSystem Define a coordinate system to specify the location. NewVector Define a vector to specify the location. NewPlane Define a plane to specify the location. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-