ClearanceBuilderTypes Enumeration¶
NXOpen.Die.ClearanceBuilder.Types is an alias for NXOpen.Die.ClearanceBuilderTypes
-
class
NXOpen.Die.
ClearanceBuilderTypes
¶ Bases:
object
Identifies which clearance type is being created in the casting.
Enum Members
Enum Member Enum Member Description Gage Clearance will be provided encompassing gage solids. Gripper Clearance will be provided encompassing gripper, or transfer, machinery solids. Lifter Clearance will be provided encompassing interior casting lifting solids. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-