AddendumSectionUserDefinedBuilder Class¶
-
class
NXOpen.Die.
AddendumSectionUserDefinedBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Die.AddendumSectionUserDefinedBuilder
builder used to select a previously defined section or a string of objects to define the section shape.To create a new instance of this class, use
NXOpen.Die.DieCollection.CreateAddendumSectionUserDefinedBuilder()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
ReverseAnchorPoint | Returns or sets the indicator to reverse the anchor point. |
Section | Returns the objects defining the section, either a previously defined section or a string of objects defining the section shape. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateUserDefinedSection | Creates user defined addendum section based upon input to NXOpen.Die.AddendumSectionUserDefinedBuilder.Section() . |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ReverseAnchorPoint¶
-
AddendumSectionUserDefinedBuilder.
ReverseAnchorPoint
¶ Returns or sets the indicator to reverse the anchor point.
The anchor point is initially the first point of the joined string of selected objects. This is used as the starting point for the section when it is placed on the tangency curve. It can be reversed to use the other end of the string as the starting point.
-------------------------------------
Getter Method
Signature
ReverseAnchorPoint
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseAnchorPoint
Parameters: reverseAnchorPoint (bool) – New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Section¶
-
AddendumSectionUserDefinedBuilder.
Section
¶ Returns the objects defining the section, either a previously defined section or a string of objects defining the section shape.
-------------------------------------
Getter Method
Signature
Section
Returns: Return type: NXOpen.Section
New in version NX7.5.0.
License requirements: None.
Method Detail¶
CreateUserDefinedSection¶
-
AddendumSectionUserDefinedBuilder.
CreateUserDefinedSection
¶ Creates user defined addendum section based upon input to
NXOpen.Die.AddendumSectionUserDefinedBuilder.Section()
.Signature
CreateUserDefinedSection()
Returns: user defined section curve Return type: NXOpen.Curve
New in version NX7.5.0.
License requirements: None.
Validate¶
-
AddendumSectionUserDefinedBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.