AddendumSectionBuilderSurfaceBuildType Enumeration¶
NXOpen.Die.AddendumSectionBuilder.SurfaceBuildType is an alias for NXOpen.Die.AddendumSectionBuilderSurfaceBuildType
-
class
NXOpen.Die.
AddendumSectionBuilderSurfaceBuildType
¶ Bases:
object
The settings to indicate the surface type.
Enum Members
Enum Member Enum Member Description NoSurface Do not create a surface. Sectional Create sectional sweep surface. CurveMesh Create curve mesh surface. ChannelTunnelCap Create channel tunnel cap surface. MultipleFaceBlend Create multiple face blend surface. WallsOnly Create walls only surface. DiskFaceBlend Create disc blend surface. SphereFaceBlend Create spherical blend surface. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-