AddendumSectionBuilderSegmentType Enumeration¶
NXOpen.Die.AddendumSectionBuilder.SegmentType is an alias for NXOpen.Die.AddendumSectionBuilderSegmentType
-
class
NXOpen.Die.
AddendumSectionBuilderSegmentType
¶ Bases:
object
The settings to indicate the segment type to update.
Enum Members
Enum Member Enum Member Description Plus Update plus segment. Punch Update punch segment. FirstStretchWall Update first stretch wall segment. Reverse Update reverse segment. TrimLedge Update trim ledge segment. DiePunch Update die punch segment. SecondStretchWall Update second stretch wall segment. DieReverse Update die reverse segment. FlatToBead Update flat to bead segment. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-