AddendumSectionBuilderSectionShapeType Enumeration¶
NXOpen.Die.AddendumSectionBuilder.SectionShapeType is an alias for NXOpen.Die.AddendumSectionBuilderSectionShapeType
-
class
NXOpen.Die.
AddendumSectionBuilderSectionShapeType
¶ Bases:
object
The settings to indicate the section shape.
Enum Members
Enum Member Enum Member Description Basic Section consists of all segments in a step like shape. DrawBar Section consists of all segments in a draw bar shape. Simple Section consists of trim ledge, punch radius, and second stretch wall segments. Channel Section consists of all segments in a channel shape. Blend Section consists of a single radius type segment to define the blend shape. Extension Section consists of a plus segment only. System Section shape determined by blending neighboring sections. UserDefined Section shape is user defined. Reuse Section shape is read from reuse library. Blank No section shape. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-