AddendumSectionBuilderSectionOrientationType Enumeration¶
NXOpen.Die.AddendumSectionBuilder.SectionOrientationType is an alias for NXOpen.Die.AddendumSectionBuilderSectionOrientationType
-
class
NXOpen.Die.
AddendumSectionBuilderSectionOrientationType
¶ Bases:
object
The settings to indicate the section orientation.
Enum Members
Enum Member Enum Member Description Default Orient perpendicular to tangency curve. ThreeDPerpendicular Orient 3D perpendicular to tangency curve Conjugate Use conjugate orientation. Isoparametric Orient along isoparametric line of closest face. IncidentEdge Orient from incident edge. Blank No orientation. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-