AddendumSectionBuilderSectionLocationType Enumeration¶
NXOpen.Die.AddendumSectionBuilder.SectionLocationType is an alias for NXOpen.Die.AddendumSectionBuilderSectionLocationType
-
class
NXOpen.Die.
AddendumSectionBuilderSectionLocationType
¶ Bases:
object
The settings indicating the location of the section being created.
Enum Members
Enum Member Enum Member Description AtPoint Create section at a point. AtPlane Create section at a plane. WithCurve Create section by approximating curves. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-