TitleBlockCollection Class¶
-
class
NXOpen.Diagramming.
TitleBlockCollection
¶ Bases:
object
Represents a collection of Title Block.
To obtain an instance of this class, refer to
NXOpen.Diagramming.DiagrammingManager
New in version NX11.0.1.
Methods¶
Method | Description |
---|---|
CreateDefineTitleBlockBuilder | Creates a NXOpen.Diagramming.DefineTitleBlockBuilder . |
CreatePopulateTitleBlockBuilder | Creates a NXOpen.Diagramming.PopulateTitleBlockBuilder . |
FindObject | Finds the NXOpen.Diagramming.TitleBlock with the given identifier as recorded in a journal. |
Method Detail¶
CreateDefineTitleBlockBuilder¶
-
TitleBlockCollection.
CreateDefineTitleBlockBuilder
¶ Creates a
NXOpen.Diagramming.DefineTitleBlockBuilder
.Signature
CreateDefineTitleBlockBuilder(titleBlock)
Parameters: titleBlock ( NXOpen.Diagramming.TitleBlock
) –NXOpen.Diagramming.TitleBlock
to be edited, if None then create a new oneReturns: Return type: NXOpen.Diagramming.DefineTitleBlockBuilder
New in version NX11.0.1.
License requirements: None.
CreatePopulateTitleBlockBuilder¶
-
TitleBlockCollection.
CreatePopulateTitleBlockBuilder
¶ Creates a
NXOpen.Diagramming.PopulateTitleBlockBuilder
.Signature
CreatePopulateTitleBlockBuilder(titleBlocks)
Parameters: titleBlocks (list of NXOpen.Diagramming.TitleBlock
) –Returns: Return type: NXOpen.Diagramming.PopulateTitleBlockBuilder
New in version NX11.0.1.
License requirements: None.
FindObject¶
-
TitleBlockCollection.
FindObject
¶ Finds the
NXOpen.Diagramming.TitleBlock
with the given identifier as recorded in a journal.An exception will be thrown if no object can be found with given name.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: NXOpen.Diagramming.TitleBlock
with this name.Return type: NXOpen.Diagramming.TitleBlock
New in version NX11.0.1.
License requirements: None.