TitleBlockCellBuilder Class¶
-
class
NXOpen.Diagramming.
TitleBlockCellBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a builder to edit
NXOpen.Diagramming.TitleBlock
’s cellThis is a sub-builder class and cannot be directly instantiated
New in version NX11.0.1.
Properties¶
Property | Description |
---|---|
Label | Returns or sets the cell label |
Lock | Returns or sets the lock status |
Tag | Returns the Tag for this object. |
Value | Returns or sets the editable text of the cell |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Label¶
-
TitleBlockCellBuilder.
Label
¶ Returns or sets the cell label
-------------------------------------
Getter Method
Signature
Label
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Label
Parameters: label (str) – New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
Lock¶
-
TitleBlockCellBuilder.
Lock
¶ Returns or sets the lock status
-------------------------------------
Getter Method
Signature
Lock
Returns: Return type: bool New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Lock
Parameters: lockStatus (bool) – New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
Value¶
-
TitleBlockCellBuilder.
Value
¶ Returns or sets the editable text of the cell
-------------------------------------
Getter Method
Signature
Value
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Value
Parameters: text (str) – New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
TitleBlockCellBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.